Tool/software: Code Composer Studio
Hi TI Engineers,My request is as below:
1,Load Image command in C2000 Gang Programmer (C2000-GANG) User's Guide's page54 is how to use by RS232 communication?As don‘t know some bytes meas in command,such as "n" ,"n-6" and "D2...Dn-6",so don't know how to write commad
Load Image command:Tx -> 3E 43 n n A1 A2 A3 0 n-6 0 D1 ... Dn-6 CKL CKH
2,What is Command about Program image from C2000-MEM TO Target flash?
3,After Program image from C2000-MEM To Target flash is finish with command or GUI, have log file to generate? If have log file, This will easy to auto judge program result by program.
Would you help reply Above questions,thanks.