Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software: TI-RTOS
Hi,
I want to configure an SCI Rx interrupt in a SYS/BIOS project. Right now I have implemented it by integrating driverlib into the SYS/BIOS project and using driverlib routines following driverlib sci loopback example.
But I have seen within SYS/BIOS pie example the next function header:
/* * ======== PIE_post ======== * This function is used to manually trigger a PIE interrupt by writing * directly to the PIEIFR register. * * Calling this function will simulate the triggering of a peripheral * interrupt. In a real world app, this function would not be needed as the * interrupt would be triggered automatically by the hardware peripheral * itself. */
Then I wonder how can I configure the pie to trigger my ISR when anything is received through some SCI port without using driverlib (only using SYS/BIOS). Can anyone tell how?
I don't want to use neither C2000Ware bitfield support nor ControlSUITE.
Thanks in advance!
Best regards,
Adria