Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: CONTROLSUITE
Hello Motor control team,
Can I use a different induction motor to work with a kit set other than HVACIMTR?
What should be done for this?
Do I need to change settings in controlSUITE?
Or the program will automatically determine the motor parameters?
Engine 127/220 V, 180 W, network frequency 50 Hz.