This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMO / eSMO HVPMSM_Sensorless



Hello,

I'm working with a f28377 microcontroler to control a PMSM motor.

We use many feedback like resolver, serial, QEP... Exactly what is done with the TMDSIDDK_v2.0

Now we want try a solution without any feedback.

To this, TI provide an exemple HVPM_Sensorless which use the SMO library. On this forum, I found the eSMO library compiled for the f28335 with FPU32.

I tested both and compare with motor angle provided by the already implemented feedback.

I found many issue which is bloquant for us:

- In reverse sense, the estimated angle SMO/eSMO has shift of 0.5.

- On motor deceleration, (so brutal then motor current pass trough 0 and motor can become like a generator) the angle switch to a very bad value.

- When motor running, I try to switch from the real feedback to the estimated feedback, this run but it is very not stable. As soon as we apply a torque on the motor axis the control Loop come crazy.

SMO / eSMO give same result.

Please is my observation are the convenient of this method or Can I change something to perform this algorithm?