Part Number: CCSTUDIO-C2000
Other Parts Discussed in Thread: TMS320F28027
Tool/software: Code Composer Studio
Hello,
I made a board for TMS320F28027 with a ARM 10pin header.
The J-link with the olimex adapter should work but I don't see it as available debuggers in the project properties. I installed it and it is available for other families of MCU's like MSP432's.
I also have a board which has the XDS110 on it, with two ARM10 jtag headers and that also does not work. It also backpowers the board for some reason. (probably VTarget connected directly to 3.3v). It fails connection test, similar to what happens if you invert the cable.
Any ideas on a way to program except known solutions:
- Buy XDS100v2 jtag probe
-Buy XDS110 / 200 jtag probe
- Use a launchpad as debugger (has no header and I am doing that already).
BR
Valerian Sarbu