Part Number: TMS320F28374D
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
HI everybody ,
I have been coding and debugging on dual core since many months no issue at all . I am on CCS8.2 and latest libs .
now I got a "strange" issue I do not understand .
when debugging code ( code is in flash ) for first time after power on CPU2 starts in a wrong way ( cputimer1 seems not starting at all even if code is runnig -->I can pause code , play again but no way , task using cputimer not running ) . only way to solve this issue is to reset and restart at least twice CPU2 and from that on everything is fine... please consider CPU1 is working alll the times no issue .
please consider :
- device stand alone ( no emulator connected ) --> device is working fine 100% on every single power on
- this issue popped up after I reserved more RAM to CPU2 ( default not enough for me ) . and 1xADC ,1xUART and 1xSPI to core 2
( if needed I can share code offline ) : could I have done something wrong ? what to check ?
questions:
- do you have a working code example in flash with dedicated resources and more memory to CPU2 I can cross check ?
-what could be the root cause to double check ?
any suggestion is welcome
thank you
regards
Carlo