This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28379D: Adding PID contoller to the eQEP speed measurement example

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

Hello everyone.

I added to the "eqep_pos_speed" C2000ware example a pid controller wich I took from the DCL C2000ware library, I added all neccssary files and headears and the programm is building and debugging without any problem.

this example take PWM1A and PWM1B to simulate the eQEP periphal. so the speed measured at the end by this example is 300 rpm.

I want to change this speed to 500 rpm trough using PID, so I added the following lines in the interrupt function :

yk = (float) qep_posspeed.SpeedRpm_fr; //reading the speed (300 rpm)
uk = DCL_runPID_C3(&pid1, rk, yk, 1.0f); // calculate the PID command

(I changed the referrence rk to rk=500.0f )

but in the debbug session the command uk is always equal to uk=1.0 and it doesn't change at all.

I don't know what I'm missing here in the program.

here is main file.c : 

//### ########################################################################
//
// FILE:    Eqep_pos_speed.c fgjnoierjgel
//
// TITLE:    EQEP Speed and Position measurement
//
//! \addtogroup cpu01_example_list
//! <h1>EQEP Speed and Position Measurement (Eqep_pos_speed)</h1>
//!
//! This example provides position measurement,speed measurement using the
//! capture unit, and speed measurement using unit time out. This example
//! uses the IQMath library. It is used merely to simplify high-precision
//! calculations.
//! The example requires the following hardware connections from EPWM1 and
//! GPIO pins (simulating QEP sensor) to QEP peripheral.
//!    - GPIO20/eQEP1A <- GPIO0/ePWM1A (simulates eQEP Phase A signal)
//!    - GPIO21/eQEP1B <- GPIO1/ePWM1B (simulates eQEP Phase B signal)
//!    - GPIO23/eQEP1I <- GPIO4 (simulates eQEP Index Signal)
//!
//! See DESCRIPTION in Example_posspeed.c for more details on the calculations
//! performed in this example.
//! In addition to this file, the following files must be included in this
//! project:
//!    - Example_posspeed.c - includes all eQEP functions
//!    - Example_EPwmSetup.c - sets up ePWM1A and ePWM1B as simulated QA and QB
//!                            encoder signals
//!    - Example_posspeed.h - includes initialization values for pos and speed
//!                           structure
//!
//! Note:
//!    - Maximum speed is configured to 6000rpm(BaseRpm)
//!    - Minimum speed is assumed at 10rpm for capture pre-scalar selection
//!    - Pole pair is configured to 2 (pole_pairs)
//!    - QEP Encoder resolution is configured to 4000counts/revolution
//!      (mech_scaler)
//!    - Which means: 4000/4 = 1000 line/revolution quadrature encoder
//!      (simulated by EPWM1)
//!    - EPWM1 (simulating QEP encoder signals) is configured for 5kHz
//!      frequency or 300 rpm (=4*5000 cnts/sec * 60 sec/min)/4000 cnts/rev)
//!    - SPEEDRPM_FR: High Speed Measurement is obtained by counting the QEP
//!                   input pulses for 10ms (unit timer set to 100Hz).
//!    - SPEEDRPM_FR = (Position Delta/10ms) * 60 rpm
//!    - SPEEDRPM_PR: Low Speed Measurement is obtained by measuring time
//!                   period of QEP edges. Time measurement is averaged over
//!                   64edges for better results and capture unit performs the
//!                   time measurement using pre-scaled SYSCLK
//!    - Pre-scaler for capture unit clock is selected such that capture timer
//!      does not overflow at the required minimum RPM speed.
//!
//! \b External \b Connections \n
//!   - Connect eQEP1A(GPIO20) to ePWM1A(GPIO0)(simulates eQEP Phase A signal)
//!   - Connect eQEP1B(GPIO21) to ePWM1B(GPIO1)(simulates eQEP Phase B signal)
//!   - Connect eQEP1I(GPIO23) to GPIO4 (simulates eQEP Index Signal)
//!
//! \b Watch \b Variables \n
//!  - qep_posspeed.SpeedRpm_fr - Speed meas. in rpm using QEP position counter
//!  - qep_posspeed.SpeedRpm_pr - Speed meas. in rpm using capture unit
//!  - qep_posspeed.theta_mech  - Motor mechanical angle (Q15)
//!  - qep_posspeed.theta_elec  - Motor electrical angle (Q15)
//!
//
//###########################################################################
// $TI Release: F2837xD Support Library v3.05.00.00 $
// $Release Date: Thu Oct 18 15:48:42 CDT 2018 $
// $Copyright:
// Copyright (C) 2013-2018 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "F28x_Project.h"
#include "Example_posspeed.h"
#include "DCLF32.h"


//
// Globals
//
// global  variables
long IdleLoopCount = 0;
long IsrCount = 0;
float rk;
float yk;
float lk;
float uk;
DCL_PID pid1 = PID_DEFAULTS;
float Duty;
POSSPEED qep_posspeed=POSSPEED_DEFAULTS;
Uint16 Interrupt_Count = 0;

//
// Function Prototypes
//
void initEpwm();
__interrupt void prdTick(void);

//
// Main
//
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
   InitSysCtrl();

//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to its default state.
//
// InitGpio();  // Skipped for this example

//
// For this case only init GPIO for eQEP1 and ePWM1
// This function is found in F2837xD_EQep.c
//
   InitEQep1Gpio();
   InitEPwm1Gpio();
   EALLOW;
   GpioCtrlRegs.GPADIR.bit.GPIO4 = 1; // GPIO4 as output simulates Index signal
   GpioDataRegs.GPACLEAR.bit.GPIO4 = 1;  // Normally low
   EDIS;

//
// Step 3. Clear all __interrupts and initialize PIE vector table:
// Disable CPU __interrupts
//
   DINT;

//
// Initialize the PIE control registers to their default state.
// The default state is all PIE __interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
   InitPieCtrl();

//
// Disable CPU __interrupts and clear all CPU __interrupt flags:
//
   IER = 0x0000;
   IFR = 0x0000;

//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the __interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
   InitPieVectTable();

//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
   EALLOW;  // This is needed to write to EALLOW protected registers
   PieVectTable.EPWM1_INT= &prdTick;
   EDIS;    // This is needed to disable write to EALLOW protected registers

//
// Step 4. Initialize all the Device Peripherals:
//
   initEpwm();  // This function exists in Example_EPwmSetup.c

	/* initialise controller variables */
    pid1.Kp = 9.0f;
   	pid1.Ki = 0.015f;
   	pid1.Kd = 0.35f;
   	pid1.Kr = 1.0f;
   	pid1.c1 = 188.0296600613396f;
   	pid1.c2 = 0.880296600613396f;
   	pid1.d2 = 0.0f;
   	pid1.d3 = 0.0f;
   	pid1.i10 = 0.0f;
   	pid1.i14 = 1.0f;
   	pid1.Umax = 1.0f;
   	pid1.Umin = -1.0f;

   	rk = 500.0f;								// initial value for control reference
   	lk = 1.0f;								// control loop not saturated
//
// Step 5. User specific code, enable __interrupts:
// Enable CPU INT1 which is connected to CPU-Timer 0:
//
   IER |= M_INT3;

//
// Enable TINT0 in the PIE: Group 3 __interrupt 1
//
   PieCtrlRegs.PIEIER3.bit.INTx1 = 1;

//
// Enable global Interrupts and higher priority real-time debug events:
//
   EINT;   // Enable Global __interrupt INTM
   ERTM;   // Enable Global realtime __interrupt DBGM

   qep_posspeed.init(&qep_posspeed);

   for(;;)
   {
   }
}

//
// prdTick - EPWM1 Interrupts once every 4 QCLK counts (one period)
//
__interrupt void prdTick(void)
{
    Uint16 i;
   //
   // Position and Speed measurement
   //
   qep_posspeed.calc(&qep_posspeed);
   yk = (float) qep_posspeed.SpeedRpm_fr;
   uk = DCL_runPID_C3(&pid1, rk, yk, 1.0f);
   Duty = (uk / 10.0f) * (float) EPwm1Regs.TBPRD;
   //
   // Control loop code for position control & Speed control
   //
   Interrupt_Count++;

   //
   // Every 1000 __interrupts(4000 QCLK counts or 1 rev.)
   //
   if (Interrupt_Count==1000)
   {
       EALLOW;
       GpioDataRegs.GPASET.bit.GPIO4 = 1; // Pulse Index signal  (1 pulse/rev.)
       for (i=0; i<700; i++)
       {
       }
       GpioDataRegs.GPACLEAR.bit.GPIO4 = 1;
       Interrupt_Count = 0;               // Reset count
       EDIS;
   }

   //
   // Acknowledge this __interrupt to receive more __interrupts from group 1
   //
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
   EPwm1Regs.ETCLR.bit.INT=1;
}

//
// End of file
//

  • Hi Hakacm,

    I am working to find the appropriate expert to help you. This may take some time to reach the right person depending on availability. Please expect an update after the weekend. I appreciate your patience.
  • It seems very likely the controller is saturating. If you consider just the proportional path for a moment: the output is (500 - 300) * 9 = 1,800, yet the controller is clamped at 1.0 because

    pid1.Umax = 1.0f;
    pid1.Umin = -1.0f;

    Think about the numerical ranges at the inputs and outputs of the controller. I suggest you normalise the reference and feedback so you are dealing with "per unit" values at the error; in other words, scale rk and yk so they always lie in the range -0.5f to +0.5f.

    That is: rk/(2*x) and yk/(2*x), where 'x' is the fastest rpm you want.

    Regards,

    Richard
  • Hi Hakacm,

    It has been a while since our reply. Let us know if your concern is resolved so we can close this thread. Thanks.