Part Number: TMS320F2812
Tool/software: Code Composer Studio
My program mainly adds the bootloader function before _c_int00. Its main function is to take two from three and move the result from flash to ram area. Therefore, in the file DSP28xx_CodeStartBranch.asm, I change LB _c_int00 to LB _bootloader, as a result, the program can run normally,which is in internal boot(the location 0x3f7ff6 in flash memory) . Now, I want to call SPI_boot function to load copysection from the external EEPROM, the program is still in the internal flash, according to the datasheet(SPRU095C), we design the external interface and general structure of source program data stream, the program can successfully run. In order to judge that the successful boot is SPI_boot, I shield the LB_bootloader in the DSP28XX_CodeStartBranch.asm (in order to shield the internal boot), As a result, the external EEprom can normally copy the codes into the specified ram area, but the program does not run successfully, so I suspect that the internal boot is still running, but I set the SPI_boot, which results in conflict with my expectation.
#pragma CODE_SECTION(bootloader, "copysections");
extern void c_int00();
// Prototype statements for functions found within this file.
interrupt void eva_timer1_isr(void);
void init_eva_timer1(void);
//extern unsigned int cinit_loadstart;
extern unsigned int cinit_runstart;
//extern unsigned int cinit_size;
//extern unsigned int const_loadstart;
extern unsigned int const_runstart;
//extern unsigned int const_size;
//extern unsigned int econst_loadstart;
extern unsigned int econst_runstart;
//extern unsigned int econst_size;
//extern unsigned int pinit_loadstart;
extern unsigned int pinit_runstart;
//extern unsigned int pinit_size;
//extern unsigned int switch_loadstart;
extern unsigned int switch_runstart;
//extern unsigned int switch_size;
//extern unsigned int text_loadstart;
extern unsigned int text_runstart;
//extern unsigned int text_size;
//extern unsigned int IQmath_loadstart;
extern unsigned int IQmath_runstart;
//extern unsigned int IQmath_size;
//extern unsigned int Flash28_API_LoadStart;
//extern unsigned int Flash28_API_size;
extern unsigned int RamfuncsRunStart;
//extern unsigned int cinit_loadend;
//extern unsigned int const_loadend;
/* extern unsigned int pinit_loadend; */
/* extern unsigned int econst_loadend; */
/* extern unsigned int switch_loadend; */
/* extern unsigned int text_loadend; */
/* extern unsigned int IQmath_loadend; */
/* extern unsigned int FlashfuncsLoadEnd; */
#define LoadADDRStartA_cinit_loadstart 0x003df77c //1
#define LoadADDRStartA_const_loadstart 0x003f8000
#define LoadADDRStartA_econst_loadstart 0x003e0da8
#define LoadADDRStartA_pinit_loadstart 0x003f8000
#define LoadADDRStartA_switch_loadstart 0x003f8000
#define LoadADDRStartA_text_loadstart 0x003dc000
#define LoadADDRStartA_IQmath_loadstart 0x003e089f
#define LoadADDRStartA_ramfuncs_loadstart 0x003e0cf2
#define LoadADDRStartB_cinit_loadstart 0x003e777c //2
#define LoadADDRStartB_const_loadstart 0x003f8000
#define LoadADDRStartB_econst_loadstart 0x003e8da8
#define LoadADDRStartB_pinit_loadstart 0x003f8000
#define LoadADDRStartB_switch_loadstart 0x003f8000
#define LoadADDRStartB_text_loadstart 0x003e4000
#define LoadADDRStartB_IQmath_loadstart 0x003e889f
#define LoadADDRStartB_ramfuncs_loadstart 0x003e8cf2
#define LoadADDRStartC_cinit_loadstart 0x003ef77c //3
#define LoadADDRStartC_const_loadstart 0x003f8000
#define LoadADDRStartC_econst_loadstart 0x003f0da8
#define LoadADDRStartC_pinit_loadstart 0x003f8000
#define LoadADDRStartC_switch_loadstart 0x003f8000
#define LoadADDRStartC_text_loadstart 0x003ec000
#define LoadADDRStartC_IQmath_loadstart 0x003f089f
#define LoadADDRStartC_ramfuncs_loadstart 0x003f0cf2
#define LoadADDR_cinit_length 0x0bd2
#define LoadADDR_const_length 0
#define LoadADDR_econst_length 0x046
#define LoadADDR_pinit_length 0
#define LoadADDR_switch_length 0
#define LoadADDR_text_length 0x1cf7
#define LoadADDR_IQmath_length 0x2c7
#define LoadADDR_ramfuncs_length 0xb5
void bootloader(void)
{
unsigned int *SourceAddr;
unsigned int *DestAddr;
unsigned int *SourceAddrB;//=(unsigned int *)LoadADDRStartB;
unsigned int *SourceAddrC;//=(unsigned int *)LoadADDRStartC;
unsigned int tmp=0;
tmp = (unsigned int)LoadADDR_text_length;
// tmp =(unsigned int)text_size;
DestAddr=&text_runstart;
// SourceEndAddr=&text_loadstart+&text_size;
// SourceEndAddr=&text_loadend;
SourceAddr=(unsigned int *)LoadADDRStartA_text_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_text_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_text_loadstart;
/* SourceAddr=&text_loadstart;
SourceAddrB =(unsigned int *)(&text_loadstart+LoadADDR_text_offsetB);
SourceAddrC =(unsigned int *)(&text_loadstart+LoadADDR_text_offsetC); */
//while(SourceAddr < SourceEndAddr)
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
tmp = (unsigned int)LoadADDR_cinit_length;
// SourceAddr=&cinit_loadstart;
DestAddr=&cinit_runstart;
// SourceEndAddr=&cinit_loadstart+&cinit_size;
// SourceEndAddr=&cinit_loadend;
SourceAddr=(unsigned int *)LoadADDRStartA_cinit_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_cinit_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_cinit_loadstart;
// SourceAddrB =(unsigned int *)(&cinit_loadstart+LoadADDR_cinit_offsetB);
// SourceAddrC =(unsigned int *)(&cinit_loadstart+LoadADDR_cinit_offsetC);
//while(SourceAddr < SourceEndAddr)
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
tmp =(unsigned int) LoadADDR_const_length;
DestAddr=&const_runstart;
SourceAddr=(unsigned int *)LoadADDRStartA_const_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_const_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_const_loadstart;
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
tmp = (unsigned int)LoadADDR_econst_length;
DestAddr=&econst_runstart;
SourceAddr=(unsigned int *)LoadADDRStartA_econst_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_econst_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_econst_loadstart;
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
tmp = (unsigned int)LoadADDR_pinit_length;
DestAddr=&pinit_runstart;
SourceAddr=(unsigned int *)LoadADDRStartA_pinit_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_pinit_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_pinit_loadstart;
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
tmp = (unsigned int)LoadADDR_switch_length;
DestAddr=&switch_runstart;
SourceAddr=(unsigned int *)LoadADDRStartA_switch_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_switch_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_switch_loadstart;
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
tmp = (unsigned int)LoadADDR_IQmath_length;
DestAddr=&IQmath_runstart;
SourceAddr=(unsigned int *)LoadADDRStartA_IQmath_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_IQmath_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_IQmath_loadstart;
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
tmp = (unsigned int)LoadADDR_ramfuncs_length;
DestAddr=&(RamfuncsRunStart);
SourceAddr=(unsigned int *)LoadADDRStartA_ramfuncs_loadstart;
SourceAddrB =(unsigned int *)LoadADDRStartB_ramfuncs_loadstart;
SourceAddrC =(unsigned int *)LoadADDRStartC_ramfuncs_loadstart;
while(tmp)
{
// *DestAddr++ = (*SourceAddr++);
*DestAddr++ = ((*SourceAddr)&(*SourceAddrB))|((*SourceAddr)&(*SourceAddrC))|((*SourceAddrB)&(*SourceAddrC));
SourceAddr++;
SourceAddrB++;
SourceAddrC++;
tmp--;
}
c_int00();
}
/*############################################################################
FILE: F281x_nonBIOS_flash.cmd
DESCRIPTION: Linker allocation for all sections.
############################################################################
Author: Tim Love
Release Date: March 2008
############################################################################*/
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAM_L0L1 : origin = 0x008000, length = 0x001d20 /* on-chip RAM */
RAM_LL : origin = 0x009d20, length = 0x0002d0 /* on-chip RAM */
RAM_LL1 : origin = 0x3F9a00, length = 0x000100
RAM_LL2 : origin = 0x3F9b02, length = 0x0001c0
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASH_I : origin = 0x3DA000, length = 0x002000 /* on-chip FLASH */
FLASH_J : origin = 0x3D8000, length = 0x002000 /* on-chip FLASH */
FLASH_GH : origin = 0x3DC000, length = 0x008000 /* on-chip FLASH */
FLASH_EF : origin = 0x3E4000, length = 0x008000 /* on-chip FLASH */
FLASH_CD : origin = 0x3EC000, length = 0x008000 /* on-chip FLASH */
FLASH_AB : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN_FLASH : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
RAM_H0 : origin = 0x3F8000, length = 0x000d00
RAM_H1 : origin = 0x3F8d00, length = 0x000660
ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
BOOT_RSVD : origin = 0x000400, length = 0x000080 /* Part of M1, BOOT rom will use this for stack */
RAMM1 : origin = 0x000480, length = 0x000320 /* on-chip RAM block M1 */
RAM_DH0 : origin = 0x3F9360, length = 0x0006a0
}
/**************************************************************/
/* Link all user defined sections */
/**************************************************************/
SECTIONS
{
/*** Code Security Password Locations ***/
csmpasswds : > CSM_PWL PAGE = 0 /* Used by file CSMPasswords.asm */
csm_rsvd : > CSM_RSVD PAGE = 0 /* Used by file CSMPasswords.asm */
/*** User Defined Sections ***/
codestart : > BEGIN_FLASH, PAGE = 0 /* Used by file CodeStartBranch.asm */
wddisable : > FLASH_GH, PAGE = 0 /* Used by file CodeStartBranch.asm */
/* copysections : > FLASH_GH, PAGE = 0 Used by file SectionCopy.asm */
/* IQmath : > RAM_LL PAGE = 0 Math Code */
IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
/*** Uninitialized Sections ***/
.stack : > RAMM0 PAGE = 1
/* .ebss : > RAMM1 PAGE = 1*/
.ebss : > RAM_DH0 PAGE = 1
.esysmem : > RAMM1 PAGE = 1
/*** Initialized Sections ***/
.cinit : LOAD = FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_H0, PAGE = 0 /* Run section from RAM */
LOAD_START(_cinit_loadstart),
LOAD_END(_cinit_loadend),
RUN_START(_cinit_runstart),
SIZE(_cinit_size)
.const : LOAD = FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_H0, PAGE = 0 /* Run section from RAM */
LOAD_START(_const_loadstart),
LOAD_END(_const_loadend),
RUN_START(_const_runstart),
SIZE(_const_size)
.econst : LOAD = FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_H0, PAGE = 0 /* Run section from RAM */
LOAD_START(_econst_loadstart),
LOAD_END(_econst_loadend),
RUN_START(_econst_runstart),
SIZE(_econst_size)
.pinit : LOAD = FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_H0, PAGE = 0 /* Run section from RAM */
LOAD_START(_pinit_loadstart),
LOAD_END(_pinit_loadend),
RUN_START(_pinit_runstart),
SIZE(_pinit_size)
.switch : LOAD = FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_H0, PAGE = 0 /* Run section from RAM */
LOAD_START(_switch_loadstart),
LOAD_END(_switch_loadend),
RUN_START(_switch_runstart),
SIZE(_switch_size)
.text : LOAD = FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_L0L1, PAGE = 0 /* Run section from RAM */
LOAD_START(_text_loadstart),
LOAD_END(_text_loadend),
RUN_START(_text_runstart),
SIZE(_text_size)
Flashfuncs : LOAD =FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = FLASH_I, PAGE = 0 /* Run section from Flash */
LOAD_START(_FlashfuncsLoadStart),
LOAD_END(_FlashfuncsLoadEnd),
RUN_START(_FlashfuncsRunStart),
SIZE(_Flashfuncs_size)
IQmath : LOAD =FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_LL, PAGE = 0 /* Run section from Flash */
LOAD_START(_IQmath_loadstart),
LOAD_END(_IQmath_loadend),
RUN_START(_IQmath_runstart),
SIZE(_IQmath_size)
copysections : LOAD = FLASH_GH, PAGE = 0 /* Load section to Flash */
RUN = RAM_LL2, PAGE = 0 /* Run section from RAM */
LOAD_START(_copysections_loadstart),
LOAD_END(_copysections_loadend),
RUN_START(_copysections_runstart),
SIZE(_copysections_size)
Flash28_API :
{
-lFlash2812_API_V210.lib(.econst)
-lFlash2812_API_V210.lib(.text)
}
LOAD = FLASH_GH, PAGE = 0
RUN = RAM_H1, PAGE = 0
LOAD_START(_Flash28_API_LoadStart),
LOAD_END(_Flash28_API_LoadEnd),
RUN_START(_Flash28_API_RunStart)
SIZE(_Flash28_API_size)
ramfuncs : LOAD = FLASH_GH, PAGE = 0
RUN = RAM_LL1, PAGE = 0
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart)
}
/******************* end of file ************************/