Could you please tell me,
(1) What is the maximum sampling rate of the F28335 Delfino board?
(2) Can it sample a physical voltage signal of 100 kHz with the precise calculation?
(3) Is the sampling rate limited by the sampling rate of ADC of the controller board?
(4) If yes, what is the sampling rate of ADC in the F28335 Delfino board?
(5) How does the resolution of the board (Bit value) depend on the sampling rate?
(6) Does the bandwidth of the sensor also limit the sampling rate?