Part Number: TMS320F28035
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi,
I am currently facing issues when trying to establish a password protection. Once I achieved to insert password properly for unlock the device, it worked, but after a blackout, the system was not longer recoverable:
My setup is the following:
- microcontroller: TMS320F28035
- debugger: XDS100 V3 REV B2
- ccs: v8.1.0.00011
- TI Uniflash: v5.0.0.2289
After reading carefully TMS320x2803x_ref_manual, and checking several threads like this one, I proceeded to create a couple of .asm files which contains:
- password protection (with no all '0's) within the PWL positions (0x3F7FF8 to 0x3F7FFF).
- 0x3F7F80 to 0x3F7FF5 addresses set to “0x0000” value in order to avoid program memory within that particular section.
password.asm file has the following code:
***************************************************
.sect "csmpasswds"
.int 0xFFFF ;PWL0 (LSW of 128-bit password)
.int 0xFFFF ;PWL1
.int 0xFFFF ;PWL2
.int 0xFFFF ;PWL3
.int 0xFFFF ;PWL4
.int 0xFFFF ;PWL5
.int 0xFFFF ;PWL6
.int 0xFFFF ;PWL7 (MSW of 128-bit password)
***************************************************
(I put values different from 0xFFFF but not all 0s)
and password_prep.asm contains the following code:
***************************************************
.sect "csm_rsvd"
.loop (3F7FF5h - 3F7F80h + 1)
.int 0x0000
.endloop
***************************************************
Both csmpasswds and csm_rsvd variables were properly linked and mapped with desired addresses:
Hence, I compiled and obtained .out file with the password protection.
After that, I connected JTAG debugger and open UniFlash tool to load corresponding image. When I browse to Memory section, if I try to check 0x3F7FF7-0x3F7FFF addresses, I could read all '0's, which means the device is in 'secure mode' (locked), which is good.
Hence, I browse to Settings & Utilities , and wrote the password that I programmed within password.asm file within the addresses 0xAE0 to 0xAE7 (key0 to key7). When I pressed Unlock button, it appeared a message in the bottom console stating that Unlock operation was successful. In order to check it, I read again 0x3F7FF7-0x3F7FFF addresses, I obtained all 'F's, which means the device is in 'unsecure mode' (unlocked). This behaviour was the expected one.
However, if I perform a blackout, and I power on the microcontoller back, I was unable to establish communication through UniFlash tool. I could not read any memory section:
I could not insert again the password for unlocking since, JTAG debugger connection is not longer successful:
Are there some errors in the steps we perform?
How could we recover the binary file or be able to load a new binary into the microcontroller?
Thanks in advance.
Guillermo