This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: SFRA does not connect to BOOSTXL-BUCKCONV demo code.

Part Number: TMS320F28069M
Other Parts Discussed in Thread: SFRA, BOOSTXL-BUCKCONV, LAUNCHXL-F28069M, CONTROLSUITE

My problem is that I cannot connect the SFRA in the demo project Buck_VMC_F28069M for the BOOSTXL-BUCKCONV with the LAUNCHXL-F28069M. I am using these tools:

  • CCS: Version 9.0.1.00004
  • ControlSuite v3.4.9
  • C:\ti\controlSUITE\development_kits\BOOSTXL_BUCKCONV\v1_01_00_00\Buck_VMC_F28069M

I can connect to the Launchpad OK, program it, and debug it.  So I've got communication over the USB to JTAG.  

Here are some screen shots of the SFRA and the device manager:

Setting up the SFRA connection.  The LaunchPad is on Com1.

  

Connection doesn't work.  The CCS connects and debugs fine.  The SFRA GUI will not connect, regardless of whether CCS is connected and in debug mode, or not connected.

  

The Device Manager with the LaunchPad connected.  Observe the COM1, a USB Composite Device that is linked to Port 1, and two Texas Instrument Debug Probes.

  

Properties of the USB Composite Device on Port 1.

  

The device manager with the LaunchPad unplugged.  COM1 is still listed.  The USB Composite Device associated with Port 1 is gone, as are the Texas Instrument Debug Probes.

 

The SFRA is a key piece of this project, so I would very much appreciate help getting it running.

Thanks,

Ciaran