This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: tms320f28379

Part Number: TMS320F28379D

Was not there a 3kW design guide for Full Bridge LLC topology using TMS320F28379 Delfino MCU?

I cannot find it in any search I did.

If there weren't any, I may have mixed up one with another...

In any event: the question then is can I parallel  Interleaved FB-LLC until I get 10kW with 30V output from 300V input?

just asking...

robin