Part Number: TMS320F28062
Hello e2e,
Target : TMS320F28062
Boot mode : Parallel IO
IDE : Code Composer Studio v6.1.2.00015 & v8.3.1.00004
Code Runs in : RAM Memory
Problem:
I am having an issue unlocking a device with a known CSM password. I have a bootloader (downloaded to RAM via Parallel IO boot mode) that can be used by our 3rd party production flash programmer to erase, program, & read/verify the Flash memory (003E8000h - 003F7FFFh).
- I have programmed locations 003F7F80h - 003F7FF5h with all 00's as indicated by SPRUH18G.
- I programmed a simple password into the CSM range:
-
-
- FEFFh @ 003F7FF8h
- FFFFh @ 003F7FF9h
- FFFFh @ 003F7FFAh
- FFFFh @ 003F7FFBh
- FFFFh @ 003F7FFCh
- FFFFh @ 003F7FFDh
- FFFFh @ 003F7FFEh
- FFFFh @ 003F7FFFh
-
I power on the TMS320F28062 with the boot select pins (GPIO37, GPIO34, TRST) all pulled to ground so I start in Parallel IO boot mode. I then download the bootcode generated from CCS, and in normal operations it works fine. However, once I've programmed the CSM password I will pass the parallel downloading sequence but I will seemingly not get any response from the device.
In my CCS project I have attempted to send the device my password via the GPIO I have initiated, but once again I do not get any handshake from pins I have initialized. Alternatively, I have just modified the CsmUnlock function to use the above mentioned password hardcoded into the function, but I still get no response from the handshake I am trying to use. I have been reading through the forum and user's guide, but cannot get a clear picture of the process regarding executable code, running from the RAM, downloaded via parallel IO boot mode, unlocking the device using a known CSM password. I see mention of the wait mode, but if I am trying to download my code to RAM via parallel, at what point would I need to switch form wait to parallel or back again?
Am I supposed to unlock the CSM using another method before downloading my bootloader via parallel IO? Does it matter at what point in main() should I theoretically call the CsmUnlock function? Such as before or after InitSysCtrl or initializing GPIO?
Thanks for the assistance!
---------------
Best Regards, Fernando