This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/496778?TMS320F2837xD-programming-CPU2-flash-from-RAM

Part Number: TMS320F28379D

Tool/software: Code Composer Studio

Hello,

I would like to program Flash-1 and Flash-2 of TMS320F28379D device directly from CC studio without going into the Flashpump semaphores

Is there any way I can do this? 

As an first time user I would like to program Flash-1 and Flash-2. Please help in letting me know on this can be done from CC studio.

Thanks,

Phani.M

  • Phani,

    Yes, you can program CPU1' Flash bank and CPU2's Flash bank using respective cores in CCS.

    Once you connect the device to debugger, you can simply load the program in CCS for each core - if the executable file has contents mapped to Flash, CCS will automatically call CCS Flash Plugin to load the contents to Flash.

    Let us know if you have any questions.

    Thanks and regards,
    Vamsi