This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi , everyone .
As title , My problem is motor out of control , while raising motor speed about 900 RPM.
And I find if I gave motor load , It will be spin well .
figure show the one of hall sensors signal .
I try to test higher speed in HVBLDC_sensored buildlevel 3,and same problem appeared .
I am doubt my driver circuit booststrap capacitance . (1uF & 0.1uF in parallel)
please help
The experts that wrote this are not around. However, I can give some pointers to look at. If the top side switch is ON for a long time, then the bootstrap cap may go low. Check the caps voltages.