Part Number: TMS320F28379D
Other Parts Discussed in Thread: UCD3138, UCD7138
Need help here to understand what we need to get started with Delfino. Application is 3 phase PFC, 3kW
#1 We have a "design by model " approach based upon mathworks embedded coder ecology.
#2 we will use the Delfino control card: we surely need it to connect to a PC. Through the USB?
#3 When done with model, and have a generated code, do we run the control card stand-alone?
#4 Seems the card has an emulator/debugger. So we do not need to buy third party hardware?
#5 Will the card run from a laptop?
thnx
-