F28377 documentation mentions that SPI in high speed mode can work up-to 50MHz if appropriate pins are used.
However in the technical reference manual (SPRUHM8H, page 2059), there is a note, that SPI baud rate should not exceed maximum rated GPIO toggle frequency.
Data manual for F28377 (SPRSP19, page 69) says that maximum GPIO output toggling frequency is 25MHz.
So what is really the maximum SPI frequency in High Speed mode ?