This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/DRV8312-C2-KIT: 28035

Part Number: DRV8312-C2-KIT

Tool/software: TI C/C++ Compiler

Hi,

I am using the above mentioned kit, with CC28035 ISO DIMM REV1.3 card. I have CCS 9.1.0, I did all the steps to start with, the motor runs when I set 'Enable Flag' to 1 in PM sensorless or BLDC sensorless Project. But, I cannot run the GUI, it says 'Connect target failed'. In CCS code it says 'this project was created using a version of compiler which is not currently installed - 5.2.10, c2000. 

I also tried installing older version of CCS (v4, v5, v7), but none of them is able to connect with GUI. 

Please kindly help me with this issue.

Thank You

Zubair