Part Number: DRV8312-69M-KIT
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
i have the DRV8312-69M-KIT and i want to run BLDC with sensorless trapezoidal method.
I used the code provided with ControlSuit for DRV8312-C2-KIT
C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\BLDC_Sensorless
And i changed the memory to this
FPUTABLES : origin = 0x3FD590, length = 0x0006A0 /* FPU Tables in Boot ROM */ IQTABLES : origin = 0x3FDC30, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FE780, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FE80C, length = 0x0000AA /* IQ Math Tables in Boot ROM */
I have 3 questions:
1- after testing the firmware with the KIT, the motor didn't run smoothly.
2- The Java script file for the watch variable is corrupted
3- is the firmware support Speed feedback also