Other Parts Discussed in Thread: C2000-GANG
Hello everyone,
I am using C2000-GANG Programmer to program for 28M35H52C dual-core microcontroller. Considering the security of passwords when device is secured, the PasswordLock register of which address is 0x680800 in OTP should be set to make its passwords invisible to JTAG debug. However, the optional OTP programming address of 28M35H52C must be in range from 0x681000 to 0x68101F in the Memory Option of C2000-GANG software . Therefore, when I select the .hex code file with PasswordLock register at 0x680800 , an error would be reported as ‘Code from file is out of range in selected MCU’. How can I solve this problem?
Thank you very much!