This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a strange problem with C2000TM PiccoloTM F28004x Series LaunchPadTM Development Kit. I'm trying to get the SCI communication to work but I only receive bytes if I set a breakpoint some where where I read the bytes from SCI registers. I'm using FIFO and I tried with and without interrupt but with same result. As a SCI port I'm using the virtual COM-port provided from the toolkit (Linux - ttyACM0)
Without interrupt I have to set a breakpoint to somewhere where I wait for bytes to FIFO:
Polling the RXFSST if (SciaRegs.SCIFFRX.bit.RXFFST > 0) { data_pu16 = SciaRegs.SCIRXBUF.all; (<- breakpoint here works) . . . . }
Or if I use interrupts, I have to set the breakpoint to interrupt handle routine. If I don't set breakpoint I do not get any data (it doesn't execute the path where the data handling is). I have also tried without debugger with the same result -> not receiving anything. I know that if I receive the bytes my program will answer correctly (works with breakpoint set).
SCI Init:
SciaRegs.SCICTL1.bit.SWRESET = 0; SciaRegs.SCICTL1.bit.SWRESET = 1; SciaRegs.SCICCR.all = 0u; SciaRegs.SCICCR.bit.STOPBITS = 1; SciaRegs.SCICCR.bit.PARITY = 0; SciaRegs.SCICCR.bit.PARITYENA = 0; SciaRegs.SCICCR.bit.SCICHAR = 7; // Calculate and set baudrate brr_u16 = (uint16_t)((LOW_SPEED_PERIPHERAL_CLOCK / (115200 * 8u)) - 1u); SciaRegs.SCIHBAUD.all = (brr_u16 >> 8u); SciaRegs.SCILBAUD.all = (brr_u16 & 0x00FFu); SciaRegs.SCIPRI.bit.FREESOFT = 3u; // Enable FIFO SciaRegs.SCIFFTX.bit.TXFIFORESET = 1; SciaRegs.SCIFFRX.bit.RXFIFORESET = 1; SciaRegs.SCIFFTX.bit.SCIFFENA = 1; SciaRegs.SCIFFTX.bit.SCIRST = 1; SciaRegs.SCIFFTX.bit.TXFFIL = 0; SciaRegs.SCIFFTX.bit.TXFFIENA = 1u; SciaRegs.SCIFFRX.bit.RXFFIL = 1u; SciaRegs.SCIFFRX.bit.RXFFIENA = 1u; SciaRegs.SCICTL1.bit.TXENA = 1; SciaRegs.SCICTL1.bit.RXENA = 1; SciaRegs.SCICTL1.bit.SWRESET = 1; SciaRegs.SCIFFTX.bit.TXFIFORESET = 1; SciaRegs.SCIFFRX.bit.RXFIFORESET = 1; // Sw reset module SciaRegs.SCICTL1.bit.SWRESET = 0; SciaRegs.SCICTL1.bit.SWRESET = 1; // Enable transfer interrupt EALLOW; PieCtrlRegs.PIEIER9.all |= 0x0001; // Only if interrupt allowed PieCtrlRegs.PIEIER9.all |= 0x0002; IER |= M_INT9; // Enable CPU Interrupt group 9 EDIS; // Configure RX pin GPIO_SetupPinMux(28, GPIO_MUX_CPU1, 1); GPIO_SetupPinOptions(28, GPIO_INPUT, GPIO_ASYNC); // Configure TX pin GPIO_SetupPinMux(29, GPIO_MUX_CPU1, 1); GPIO_SetupPinOptions(29, GPIO_OUTPUT, GPIO_ASYNC);
Any ideas?
Hi Juhis,
I don't see anything obviously wrong based on a cursory read through your code.
You might try starting with the SCI fifo loopback code that exists in c2000ware for the F2837xD device. You should be able to drop the SCI portions of that code into a F2804x project with minimal changes. Once you get it to function correctly in loop-back mode, disable the loop-back and instead supply the data from your external source.
Hi Juhis,
I'm going to mark this thread as 'TI Thinks Resolved'. Feel free to post back to this thread to confirm if you were able to solve the issue or need additional help. If the thread locks, use the 'Ask a related question' button to continue the discussion.