Other Parts Discussed in Thread: TMDSCNCD28027
Tool/software: Code Composer Studio
Hello everyone!
I face pretty strange behavior of mcu.
1. I set CSM password different from all ones
2. Then program mcu.
3. Then I tried to check if code protection works - I set wrong key in key register Properties->Debug->Flash settings, and in "Flash Program Setting" I set Verify Only
4. Then I start debug session and got in console window something like - ... GEL ..can't calibrate device... device is locked... e.t.c.
5. After that I can't connect to the mcu irrespectible of values in CSM keys.. And get "Error connecting to the target: (Error -1135 @ 0x0)" error...
This happens twice on two mcu's. Before setting CSM password everything was ok with connecting and debugging.
No reloading or resetting helps..
I'm using CCS Version: 8.3.0.00009, XDS100v1.
MCU works ok.