Part Number: TMS320F28379D
Other Parts Discussed in Thread: REF3130
Hi,
I wanna use one of the CMPINxP pins to monitor the overvoltage event. and CMPINxN Will be controlled by internal DAC. Regarding this, I have a few doubts.
- CMPSS DAC's are dedicated and not one of 3 DAC on the Device.
- If CMPINxN is driven by internal DAC then, Can I use that CMPINxN pin for other ADC read Functionality or do I need to leave that pin floating?
- I am doing a voltage read on the "ADCINC2 / CMPIN6P" pin. Now if I wanna use continues voltage reading as well as this Overvoltage monitoring using Comparator, is it possible to do it on this single pin or I need to connect the same signal to a dedicated CMP pin?
Regards
Vishal kakade