Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Dear TI community,
I have just started my journey with LAUNCHXL-F280049C and my question is regarding CAN interface or any other external or internal method, which can help me do the following:
what I need to do is to generate PWM signals and being able to change the frequency and duty cycle of these PWMs during the time that the test is running. whithout any external hardware (resistors,capacitors, ...)
my idea was that I take CANape as the user interface and send CAN messages to the LAUNCHXL-F280049C through CANL and CANH pins. but I do not know how to implement and interpret these CAN messages in Code Composer. is there any example of using CAN messages?
that would be so nice if you could help me with this problem.
looking forward to hearing from you soon :)
Mohammad