Other Parts Discussed in Thread: CONTROLSUITE, , MOTORWARE
Tool/software: Code Composer Studio
Hi
I'm working with with TMS320F28069M. after i developed my application, now i want to program it into Flash instead of RAM(directly program). i found these lines in "Controlsuite" examples:(Example_2806xFlash project)
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadEnd;
extern Uint16 RamfuncsRunStart;
extern Uint16 RamfuncsLoadSize;
...
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32)&RamfuncsLoadSize);
InitFlash();
but these line does not cause MCU to standalone boot from Flash.
after i searched into Motorware projects, i found "proj_labc" project that worked correctly with standalone Flash, after i analyzed the main file, i found the difference is memory copy function, in this project, the original memcpy is not used, instead, a simple function wrote :
void memCopy(uint16_t *srcStartAddr,uint16_t *srcEndAddr,uint16_t *dstAddr)
{
while(srcStartAddr <= srcEndAddr)
{
*dstAddr++ = *srcStartAddr++;
}
return;
}
what wrong with "memcpy" function?!
i don't have any idea why "memCopy" function worked but original "memcpy" not worked!
please help me
Sincerely Rodger