Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I'm using TMS320F28388D. I'm trying to implement usb_bootloader.
In the case of 28377d, if you input key(0x5A) and usb_device_code(0x0C) at 0xD00, PC recognizes usb device.
However, in the case of 28388d, enter 0x5AFF and 0xFFFF in 0xd00 and 0xd02 as the contents changed from 28377. And if you enter 0xFF09(usb_device_code) and 0xFFFF in 0xd04 and 0xd05, the PC will be recognized as an unknown device.
Q1. If the current 28388d is shipped with the GPIO72 and GPIO84 set to High, is the USB Bootloader mode correct?
Q2. Is it normal to display Unkwon device on the PC when it is in USB Bootloader?
Q3. How can I use the USB Bootloader to get the USB information properly on my PC like the 28377d?
Q4. If the 28388d recognizes USB Bootloader, can I use the USB_Flash_programmer provided with the C2000?