Part Number: LAUNCHXL-F28379D
Hello everyone,
I have opened a thread but nobody on TI side has replied. So I opened again.
My aim is to be able to send and receive data from SCI B or SCI C by programming on MATLAB.
I want to use SCI B or SCI C which I can connect with simple jumper cables from GPIO 18-19 and GPIO 56-139. But I could not manage to get any communication signal from these ports. Only SCI A works but it is connected to the USB. I want to use SCI B and SCI C.
As far as I understand I need to change MUX to be able to use SCI B or SCI C. I do not know how to do that ?
Any help will be appreciated.
Thanks.