This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/F28M36P63C2: F28M36 Problem with comparator status query COMPSTS

Part Number: F28M36P63C2


Tool/software: Code Composer Studio

We use EPwm7, EPwm9 and EPwm11 for a 3-phase motor.
I want to switch off the PWM with the output of the comparator modules (COMxPOUT).
The comparator outputs go to trip inputs 1, 2 and 3.
Together with other trip inputs 4, 7, 8, 9, 11 a DCAEVT1 event is generated,
the PWM is switched off and an interrupt is triggered.  
In the interrupt I would like to query the COMPSTS bit
so that I know which of the 3 comparators has responded.
The query only works in the EPwm7 interrupt.
The query of the comparator status in the EPwm9 and EPwm11
interrupts does not work, although the comparator status is
the cause of the interrupt.
What is wrong?
Here is the code:
(EPwm9 and EPwm11 are initialized accordingly)


    // Define an event (DCAEVT1)                             // TRM 737
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT1  = 1;               // Map Trip input 1 comparator U to DCAH
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT2  = 1;               // Map Trip input 2 comparator V to DCAH
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT3  = 1;               // Map Trip input 3 comparator W to DCAH
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT4  = 1;               // Map Trip input 4  ERROR0 to DCAH
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT7  = 1;               // Map Trip input 7  ERROR1 to DCAH
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT8  = 1;               // Map Trip input 8  ERROR2 to DCAH
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT9  = 1;               // Map Trip input 9  ERROR3 to DCAH
    EPwm7Regs.DCAHTRIPSEL.bit.TRIPINPUT11 = 1;               // Map Trip input 11 ERROR5 to DCAH
    EPwm7Regs.DCTRIPSEL.bit.DCAHCOMPSEL = 0xF;               // DCAH = Trip combination input (all trip inputs selected by DCAHTRIPSEL register ORed together)
    EPwm7Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI;              // DCAEVT1 = DCAH high
    EPwm7Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT1;               // DCAEVT1 = DCAEVT1 (not filtered)
    EPwm7Regs.DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC;      // Take async path

    // Enable DCAEVT1 as one shot trip sources
    // Note: DCxEVT1 events can be defined as one-shot.
    //       DCxEVT2 events can be defined as cycle-by-cycle.
    EPwm7Regs.TZSEL.bit.DCAEVT1 = 1;

    // Trip zone register for event switch off EPWM outputs A + B
    EPwm7Regs.TZCTL.bit.DCAEVT1 = TZ_FORCE_LO;              // Trip action set to force-low for output A

    // Trip zone register for software switch off EPWM outputs A + B
    EPwm7Regs.TZCTL.bit.TZA = TZ_FORCE_LO;              // Trip action set to force-low for output A (TRM 725ff)
    EPwm7Regs.TZCTL.bit.TZB = TZ_FORCE_LO;              // Trip action set to force-low for output B

    // Register ISR for Trip Zone Interrupt EPWM7
    PieVectTable.EPWM7_TZINT = &epwm7_tzint_isr;
    
    // Enable CPU INT2 which is connected to EPWM1-8 INT:
    IER |= M_INT2;

    // Enable EPWM INTn in the PIE: Group 2 interrupt 7
    PieCtrlRegs.PIEIER2.bit.INTx7 = 1;

    // Enable TZ interrupt DCAEVT1
    EPwm7Regs.TZEINT.bit.DCAEVT1 = 1;

//--------------------------------------------------

__interrupt void epwm7_tzint_isr(void)
{
    if (Comp1Regs.COMPSTS.bit.COMPSTS == 1)   /* Comparator U?         */
      ERR_U = 1;               

    // Acknowledge this interrupt to receive more interrupts from group 2
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP2;
}
 
//--------------------------------------------------

    // Initialize GPIO:
    InitComp1Gpio();    // output GPIO193 --> input GPIO56
                                                // TRM 977
    Comp1Regs.COMPCTL.bit.COMPDACEN  = 1;       // Enable COMP1
    Comp1Regs.COMPCTL.bit.COMPSOURCE = 0;       // Use DAC1 as minus input to comparator
    Comp1Regs.DACVAL.bit.DACVAL   = ilim_val;  // Set DAC1 to ILIM-Value, 0...5V = 0...1023
    Comp1Regs.COMPCTL.bit.CMPINV  = 0;          // Do not invert comparator output: Output high if input A > input B
    Comp1Regs.COMPCTL.bit.SYNCSEL = 1;          // Synchronous output
    Comp1Regs.COMPCTL.bit.QUALSEL = 2;          // Filter 0...15 = 1...16 Takte @ 150MHz/4
                                                // Comparator output is Comp1Regs.COMPSTS.bit.COMPSTS

    // init trip inputs
    EALLOW;
    GpioG1TripRegs.GPTRIP1SEL.bit.GPTRIP1SEL = 56;    // Select PJ0_GPIO56 as trip input 1 for U
    EDIS;

  • Juergen,

    If the comparator input signal is related to the EPWM actuation (for example, if the comparator is monitoring the feedback from whatever the EPWM is controlling), then it is likely that the disabling of the EPWM output is also reversing the trip condition, which will cause the comparator COMPSTS to de-assert.

    For this comparator architecture, there are no in-line COMPSTS latches for the trip flag. You would need to use a spare latch from another module such as GPIO interrupt or an EPWM OST or CBC trip.

    -Tommy

  • Hi,

    the problem is that when the EPwm9 (phase V) or EPwm11 interrupt (phase W) is triggered, the comparator status flag is not yet set.  With EPwm7 (Phase U) it works.  The comparator status flags are not yet set when the interrupts are triggered, although they are the trigger of the interrupts.  Only if I wait for a while in the interrupt I will notice that the comparator status flag is set.

    The evaluation of the EPwm OST trip flags does not help me, because each comparator always switches off all three EPWMs.

    Juergen

  • Juergen,

    I think we are in general agreement about your observations and device limitations, but I am not clear on how you want the comparator + EPWM modules to behave. Please keep in mind that my area of expertise is at the device-level, not the broader system level of whatever application you are implementing.

    Here are some questions for my understanding:

    • Are your trip events considered to be part of normal activity that happens periodically or do they indicate that some fault has occurred?
    • Is there a real-time requirement for how quickly the EPWM needs to react in response to a trip event?
    • Do all three EPWMs need to react simultaneously?
    • Do the EPWM outputs have influence over the trip source?
    • Do you have any unused GPIO interrupts, EPWM modules, or EPWM DCxEVT data paths?

    -Tommy

  • Tommy,

    many thanks for your help.

    Here are more informations:
    We use EPWM7, EPWM9 and EPWM11 for a 3-phase motor.
    The comparators monitor the current limit. If this is exceeded in one comparator,
    all three EPWM should be switched off immediately and simultaneously. This works.

    At the same time, the three Trip Zone Interrupts were triggered. This also works.

    In the Trip Zone Interrupt I query the status bit COMPSTS to determine which comparator effect.
    (Comparator 1 in Trip Zone Interrupt 7, Comparator 2 in TZINT 9 or Comparator 3 in TZINT 11).
    This works only in Trip Zone Interrupt 7 (Comparator 1).

    If the three trip zone interrupts are triggered by the Comparator 2 or 3, the status bit COMPSTS
    in trip zone interrupts 9 or 11 is not set at the time of the query.
    Only if I wait for a while in trip zone interrupt 9 or 11 the status bit is set.

    I do not understand this because the comparator outputs 2 or 3 are the trigger of the Trip Zone Interrupts 9 or 11 itself!
    And so the comparator status bit must be set!

    The Trip Zone Interrupts are carried out by the comparator outputs (TRIPINPUT 1-3) and further inputs (TRIPINPUT 4,7,8,9) to DCAEVT1.

    Your questions:
    •Are your trip events considered to be part of normal activity that happens periodically or do they indicate that some fault has occurred?
    They do indicate that some fault has occurred (over current).

    •Is there a real-time requirement for how quickly the EPWM needs to react in response to a trip event?
    The EPWM7,9 and 11 should react immediately to the TRIPINPUT 1, 2 and 3 (ORed to DCAEVT1).

    •Do all three EPWMs need to react simultaneously?
    Yes.

    •Do the EPWM outputs have influence over the trip source?
    In practice yes.  At the moment I'm testing on the desk with an analog voltage at the comparator inputs.

    •Do you have any unused GPIO interrupts, EPWM modules, or EPWM DCxEVT data paths?
    EPWM are not free. DCAEVT2, DCBEVT1, DCBEVT2 are free.

    Can you explain me the delay between triggering the Trip Zone Interrupts and setting the comparator bits?

    Juergen

  • JuergenZ said:
    The comparators monitor the current limit. If this is exceeded in one comparator,
    all three EPWM should be switched off immediately and simultaneously. This works.

    I assume that you are using DCxxTRIPSEL to enable the multiple comparator TRIPINn sources to trip the EPWMs simultaneously.



    JuergenZ said:
    In the Trip Zone Interrupt I query the status bit COMPSTS to determine which comparator effect.
    (Comparator 1 in Trip Zone Interrupt 7, Comparator 2 in TZINT 9 or Comparator 3 in TZINT 11).
    This works only in Trip Zone Interrupt 7 (Comparator 1).

    If the three trip zone interrupts are triggered by the Comparator 2 or 3, the status bit COMPSTS
    in trip zone interrupts 9 or 11 is not set at the time of the query.
    Only if I wait for a while in trip zone interrupt 9 or 11 the status bit is set.

    I do not understand this because the comparator outputs 2 or 3 are the trigger of the Trip Zone Interrupts 9 or 11 itself!
    And so the comparator status bit must be set!

    A couple of things to consider:

    • There is no COMPSTS latch to retain the trip history so it would not be reliable to use this raw status in a system where the current sense might fall (due to EPWM trip behavior) below the comparator trip threshold by the time the ISR is able to execute
    • With the DCxxTRIPSEL OR'd trip inputs, each EPWM will qualify a trip when any of the enabled comparators is asserted. The trips for Comparators 2 and 3 do not need to be asserted in order for EPWMs 9 and 11 to respond.

    JuergenZ said:
    •Do the EPWM outputs have influence over the trip source?
    In practice yes.  At the moment I'm testing on the desk with an analog voltage at the comparator inputs.

    If the comparator input voltage is held near the trip threshold, the comparator output may oscillate between tripped and untripped if there is input noise. I recommend monitoring the COMPnOUT signal on the pin if instability might fit your observations. It may also be helpful to profile the COMPnOUT pin activity during the ISR when COMPSTS is being read.

    JuergenZ said:
    •Do you have any unused GPIO interrupts, EPWM modules, or EPWM DCxEVT data paths?
    EPWM are not free. DCAEVT2, DCBEVT1, DCBEVT2 are free.

    It should be possible to make use of the spare DCBxx path of each EPWM to only monitor its coupled comparator output. For example, EPWM7.DCBEVT1=TRIPIN1, EPWM9.DCBEVT1=TRIPIN2, EPWM11.DCBEVT1=TRIPIN3.

    The DCBEVT path has latched status bits that are more reliable for finding the trip source.

  • Tommy,

    I have chosen the option to trigger an interrupt for each comparator trip input via the DCBEVT1 path.

    Juergen