This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: Heating issue doubt

Part Number: TMS320F28069M
Other Parts Discussed in Thread: TMS320F28069

I have a problem with the TMS320F28069 microcontroller heating effect. Whenever I am providing power to it. it is raising its temperature which is more than the temperature of the launchPAD. I have designed the circuit using the launchpad circuit reference. Here I found a mistake which I thought this can be an issue, please tell me if this is the issue which can be causing the heating problem?

Here The inductor is different. But I have provided a different ferrite bead. which is in the following.

I have used (38) ferrite bead, for the L3 and L4 ferrites.

Is this is causing the heating problem? The temperature is rising at about 60-68 degrees Celcius.

thank you.