Part Number: TMS320F280049
Figure 12.4(P1453 in TRM)shows that the PGAx_OF is the source of CMPx_HP0 and CMPx_LP0. While take Analog Group1 for example, in Table 12-1(P1454 in TRM), if pin A2/B6/PGA1_OF is used as normal ADC input A2 and B6 (not as PGA1_OF), can this pin be used as CMP1_HP0 at the same time?