Part Number: TMS320F280049C
Other Parts Discussed in Thread: INA240, BOOSTXL-DRV8320RS
Tool/software: Code Composer Studio
It seems the real time debug is not being protected by the USB isolation boundary JP1, JP2, JP3 removed.
Question asked previous thread about x49c launch pad hardware configuration (U3) being suspect. It would seem XDS110 TM4C129x remains 3v3 powered via target side of isolation when USB isolation straps JP1,JP2,JP3 are removed. It would seem Proper USB isolation also involves +3v3 source for XDS110 being +VBUS powered via U101 and target via Booster pack headers +3v3.
1. How do we make XDS110 +3v3 fully isolated from target +3v3 booster pack power source or this some other CCS 9.1 issue with XDS110?
2. How to stop XDS110 from CCS debug disconnection when motor SDK run time GUI remains connected but produced odd offset wave shape.
3. Where is reset cause register located in TMS320F280049c or why was it omitted? And confirmed register S1 bit 1 = 0.
Error that occurs after disconnect:
C28xx_CPU1: Trouble Writing Memory Block at 0x402 on Page 1 of Length 0x1: (Error -1041 @ 0xFFFFFEFB) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.4.0.00006) 28xx_CPU1: Trouble Halting Target CPU: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.4.0.00006) C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.4.0.00006)
C28xx_CPU1: Unable to determine target status after 20 attempts C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
Scope probes during disconnect INA240 (CH2) and Phase A (CH1).