This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312-C2-KIT: DRV8312-C2-KIT

Expert 1225 points

Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: DRV8312, DRV8320

Hello,

I'd like to ask whether there is possibility to replace (on the KIT) DRV8312 driver and put another but with FETs outside, so that I can drive higher currents.

I have a FOC program generated from Simulink for the F28035 and just want NOT to change the software.

The only problem I forsee are the RESET lines. Are they necessery?

If I change the driver to DRV8320HRTV then I have to leave reset lines floating (and as I believe I'm loosing the protection)

Or maybe DRV8320 does not require additional protection as it has built-in protections and RESET signals would be redundant in that case?

I'm not asking about physical constraints as I'm going to design my own board.

Regards,

Adam

Regards,

Adam