Part Number: TMS320F28075
Hi,
In the technical reference manual for the TMS320F2807x Piccolo Microcontrollers (SPRUHM9B), there seems to be a conflict between Figures 13-22 (AQCTLR[SHDWAQAMODE]) and 13-23 (AQCTLR[SHDWAQBMODE]) and Table 13-23 (AQCTL Register Field Descriptions).
Table 13-23 states that the value 11b for the bitfields LDAQASYNC and LDAQBSYNC is reserved. It also states that the value 11b for the bitfields LDAQAMODE and LDAQBMODE will freeze the update. See the table below.
However in Figures 13-22 and 13-23 it specifies the opposite. i.e.
- 11b is reserved in bitfields LDAQAMODE and LDAQBMODE
- 11b in bitfields LDAQASYNC and LDAQBSYNC will freeze updates
See figures below.
Which is correct?
Thanks,
Fearghal Kineavy