I want to use the EMIF1 memory interface on the ControlCard HSEC8 edge connector but I don't see where Data Bit D9 is placed on the Edge Connector HSEC8.
It is on IC signal called GPIO075 but that signal does not appear on the HSEC8 connector.
I suspect it is pin 142 for the schematic calls it MCU_GPIO126.
The PDF schematic is dated Rev A, 4/11/2019