This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT: TMDSHVMTRPFCKIT

Part Number: TMDSHVMTRPFCKIT


Ramesh,

Thank you for the additional information.

I have an additional question; Since I am a novice when it comes to configuring a Low Pass Filter (LPF), my project involves measuring two phases of the TI HV Motor Drive such as phases, U-V, V-W and W-U. I know in a single phase application, the LPF is interconnected to the Line In and the Neutral. In my application, I need to measure the combined voltage of two phases (not one phase to neutral) from the two outputs of my three phase multi-switch. When measuring the combined voltage of two phases, is the configuration of the LPF and the interconnection of the LPF the same or, does it require a LPF for each of the two phases? 

Thank you,

Ron