This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1000: TIDM-1000: Compatible ControlCARDs

Part Number: TIDM-1000
Other Parts Discussed in Thread: TMDSCNCD28379D, , TMDSCNCD280049C, TMDSCNCD28388D

I have a TIDM-1000 board on the way, but I do not have a TMDSCNCD28379D ControlCARD, since they're out of stock locally.

I do have an F28M36x ControlCARD R1.1 on hand, but this isn't a part with a CLA, so I doubt it can be useful.

Are there any other supported ControlCARDs with the TIDM-1000 that I can check for local stock? For example, the TMDSCNCD280049C with a Piccolo F280049C is available. If that is possible, are there any limitations or considerations that would make it worthwhile to also get a TMDSCNCD28379D card?