Part Number: TMS320F280049C
Hi Team,
My customer now is using F280049C for a new project development, and VREGENZ PIN is in floating status by accident, and reported below 2 strange things that the code can't run, could you kindly give comments for the reason?
Case 1: Connect the F280049 with JTAG, and download the code and run without powered off, the code run well, but powered off and re-powered on with JTAG, the code couldn't run well;
Case 2: Using external LDO to powered on VDD(1.2V), using JTAG to download and run without powered off, the code couldn't run;
Expect for your reply, thanks.