Part Number: TMS320F28374D
Other Parts Discussed in Thread: C2000WARE
HI everybody ,
I m using CLA and have 3 tasks : everything is OK but then I added code ( just few lines ) and CLA hangs .
I added code in Task 3 , and have the issue . So I removed and put extra line in Task1 and got same crash : so it seems related to code size .
questions :
- do you have a working example with more than 1 task I can cross check vs mine ?
- what can I check to find this issue ?
- do you have a proper linker file I can use to be usre issue is not there ?
bets regards
Carlo