Part Number: TMS320F28388D
Hi expert,
My customer sending CAN frames in three timer triggered functions with F28388D's CM core. These "takes" who send CAN frame have an interval of 1ms, 2ms and 10ms. Data transmitting is via for loop with no special delay among each frames.
They met transmmit stop issue when running and it seems highly related to "How they send these frams", means the sending frequency. I get three register capture here and one is normal case, the other two are abnormal cases. Could you help me review the register dump to idenfity the possible casue?
Let me know if you need more information here.
Thanks
Sheldon