Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Hi everyone!
I have a query about Flash programming and running ISRs in SRAM!
Whenever I flash my code (with state machine and ISRs) it goes into (ILLEGAL ISR), why is that happening?
I am using ADC ISR for all functioning (PI, startup) and scheduling in state machine (Timer 0), how to configure the CCS settings, to run code perfectly; without falling into ILLEGAL ISR
// Here is my Main File
/*
* Main.c
*
* Created on: 01-Oct-2019
* Author: Abhinav
*/
#include "F28x_Project.h"
#include "IQmathLib.h"
//
void GpioSetup(void);
void SetupEPwm(void);
void AdcInit(void);
void InitTimer(void);
void InitINT(void);
void MAVG_Init(void);
void SSramp(void);
//
__interrupt void ISR1(void);
__interrupt void SMISR(void);
//
//
void main(void)
{
InitSysCtrl();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
GpioSetup();
InitTimer();
InitINT();
MAVG_Init();
AdcInit();
SetupEPwm();
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
EINT;
ERTM;
for(;;);
}
//
void InitINT(void)
{
InitPieVectTable();
EALLOW;
PieVectTable.ADCA1_INT = &ISR1;
PieVectTable.TIMER0_INT = &SMISR;
EDIS;
//
CpuTimer0Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0
//
IER |= M_INT1;
//
PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
}
//
Regards
Abhinav Soni