Part Number: TMS320F28069
I use 2 .c and .h files in the project,
Among them, the structure is defined in the ah file, and the structure is also defined in the bh file. I referenced the structure of bh in the ah header file and included the bh header file, but the compilation error: said that I am citing in ah The structure of bh is not defined. I included it, or it still gives an error. What is the situation? It's very unclear. I can create a new project for the same operation, but it is like this in my project. How do I set up CCS? I ccs9.2.