Part Number: TMS320F28027F
Other Parts Discussed in Thread: TMDSHVMTRINSPIN, , MOTORWARE
I have a related question on the topic "Acim motor does not reach maximum speed"
We are using the TMDSHVMTRINSPIN dev kit with the TMS320F28027F control card.
Our goal is to spin the motor at 3600rpms. To help us better understand controlling an ACIM we are using the motor shown in section 4.8 of the InstaSPIN-FOC User's Guide. We used the procedures outlined it section 4.8 to calculate the parameters and have completed the labs for FOC up to 5b.
But on the bench, with no load, the rpms top out at roughly 1300. When field weakening or powerwarp is enable higher speeds can be reached.
Questions:
1. Is it normal to have to use field weakening or powerwarp for achieve the 2x time rated speed?
2. Are there other parameters that factor into motor speed?
3. Is that more information I can provide?
Thanks,
Rob