This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have produced a new drive for us with the hvmtrkit.
By the way, there is a problem does not reach the maximum speed of the motor.
It was confirmed to be driven up to speed to lower the current value.
However, performance is not good.
Therefore, I am sure that this issue is a matter of parameter setting.
Using the 'spruhj1' document I calculated motor parameters.
but I do not know exactly correct.
Hardware filters also difficult to value accurately calculated.
I have attached a current / voltage acquisition circuit and user.h file.
Please review whether any problems at once.
I lack a lot of experience in motor control.
I think that would be a lot of problems.
Reviewed the document and tell us what went wrong.
I used the motorware project 'lab12b'instaspin.zip
you would have to use field weakening or powerwarp to achieve the 8x time rated speed you desire. It can only be done by lowering the induced magnetization. when you lower the field you are going to lose some dynamic torque response capability, so acceleration/decelerations will be more challenging. You will also need to re-tune your current controllers for stability during these operating points.