Other Parts Discussed in Thread: C2000WARE
Thanks for your support. I resolved my previous issue, but now I have slightly different issue
I am using 6 ePWMs (ePWM1 to ePWM6), all are currently working with 60kHz frequency and synchronized. I want to use ePWM5 at 20kHz all reamaing at 60kHz. Disabled the sync chain for ePWM5. But to retain the sync effect I want to introduce a offset value for ePWM5. Is there any method to calculate the offset value? When I subtracted 246 (based on 60kHz) from WA value, all PWMs are aligned properly. But I don't have any justification for this number. May be this is the delay between each ePWM.
Regards
Sajin Arakkan