This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: SPI_setConfig() function issue in spi_ex4_eeprom example and InstaSPIN hal.c

Part Number: TMS320F280049C

Hi Team,

If you look at SPI configuration in the example spi_ex4_eeprom and in the hal.c file of the InstaSPIN-FOC implementation, the set bitRate value (in comments) is different then the argument passed in the SPI_setConfig() function. This doesn't make sense because it doesn't follow the baud rate calculation explained on the page 2216 of the SPRUI33C.  

How to calculate bitRate argument for SPI_setConfig() function from the desired bitRate setting for SPI communication? Please look at the code from the both the example. 

// SPI configuration from the spi_ex4_eeprom example 

// SPI configuration. Use a 2MHz SPICLK and 8-bit word size.
//
SPI_setConfig(SPIA_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA1,
                  SPI_MODE_MASTER, 1000000, 8);


// SPI configuration from the hal.c of InstaSPIN-FOC

// SPI configuration. Use a 1MHz SPICLK and 16-bit word size. 500kbps
SPI_setConfig(obj->spiHandle[0], DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0,
                SPI_MODE_MASTER, 400000, 16);