This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Would like to understand lower level performance impact of enabling the CLA background task, i.e. the context overhead switching to a foreground task. This detail can be summarized by the elapsed time from the edge of a CLA trigger source to the first instruction of a foreground task, with and without the background task enabled. Section 8.3.4 of the TRM discusses the high level, but no cycle count impact is indicated. The CLA Software Development Guide also does not mention this detail. Suggest as an addition to these docs.
Thanks,
Eric
Eric,
Background task is running and a trigger is asserted: it takes 9 clock edges to bring the MCLA instruction of newly triggered task to D2 phase i.e MPC starts executing the new foreground task.
Note: if MBCNDD, MCCNDD, or MRCNDD are in D2 when a new task is triggered, it will take 3 more cycles to complete the uninterruptible instruction as mentioned in the TRM.
Compared to starting a normal task, there is difference of one clock cycle to force the MSTOP in D2 phase of background task before it exits as compared to normal task starting. That is, for a normal task there are 8 clock edges to bring the MCLA instruction of new task to D2 phase i.e MPC starts executing the newly triggered task.