Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Max SCI UART baud rate

Part Number: TMS320F280049C

Hello,

I'm looking in the datasheet for timing data for SCI in UART mode. What's the maximum baud rate supported on F28004X? It seems like the datasheet just skips from the intro to SPI mode without any further data on UART mode.

I found this related post for the LIN peripheral which looks like it's a SCI peripheral in disguise, does this SYSCLK/32 also apply to the regular SCI module?

Regards,
Munan

  • Hello Munan,

    Thank you for your question! I would highly recommend looking instead at our device Technical Reference Manual (located below the datasheet link on the product page, and at this link here) for in-depth information on each of the peripherals. Particularly Chapter 23, starting at page 2249, covers the SCI module and its timings, including maximum baud rate and calculations related to it.

    Let me know if this answers your question!

    Regards,

    Vince

    ----------------------------------------------------------------------------------------------------------------------------

    If I was able to answer your question, please press the green "Verified" button below, thanks!

  • Hi Vince,

    Thanks for the response, just for people looking for a quick answer the max supported baud rate is LSPCLK/16 which for F28004x is a max of 6.25 Mbps.

    Munan