Other Parts Discussed in Thread: C2000WARE
Hi, I am using the F28379D Launchpad with CCS 9.1, and when I try to connect to Target I get this issue:
- Power Levels:
3.3V pin ---> 391 mV “almost Zero volt”
5V pin ----> 4.68V
- D 1, 4, 9, 10 LEDs not working
- S1, 2, 3 Switches states: ON
- I tried to S1&2 Up while S3 down then reset but still nothing happen
- Not Connected in device Manger
- When disconnect JP1 D4 becomes ON and the device Connected in Device manager but gives