Part Number: LAUNCHXL-F28027F
Tool/software: Code Composer Studio
Hi,
I have asked sevel times this question but haven't got satisfying reply....
I am using simple example of ADC_SOC for ADC conversion. I have to use value of ADc that is read by MCU for external purpose by the help of if statement. as the value is being stored in AdcResult.ADCRESULT1 which is then stored in voltage1[conversioncount] which is array. How to access the value of ADC as variables for further use in if statement. I have tried in many ways but the error 'statemenet unreachable' is written.
I have merged ADc_SOC and HRPWM example and with the specific value of ADc i will generate specific PWM. After merging both examples, AdcResult.RESULT1 is showing some problem. At the side bar occurence with silver indication is written on it.
The example is given below with the highlighted error points...
//###########################################################################
//
// FILE: Example_2802xHRPWM.c
//
// TITLE: f2802x Device HRPWM example
//
// ASSUMPTIONS:
//
//
// This program requires the f2802x header files.
//
// Monitor ePWM1 pin on an oscilloscope as described
// below.
//
// ePWM1A is on GPIO0
// ePWM1B is on GPIO1
//
//
// As supplied, this project is configured for "boot to SARAM"
// operation. The 2802x Boot Mode table is shown below.
// For information on configuring the boot mode of an eZdsp,
// please refer to the documentation included with the eZdsp,
//
// $Boot_Table
// While an emulator is connected to your device, the TRSTn pin = 1,
// which sets the device into EMU_BOOT boot mode. In this mode, the
// peripheral boot modes are as follows:
//
// Boot Mode: EMU_KEY EMU_BMODE
// (0xD00) (0xD01)
// ---------------------------------------
// Wait !=0x55AA X
// I/O 0x55AA 0x0000
// SCI 0x55AA 0x0001
// Wait 0x55AA 0x0002
// Get_Mode 0x55AA 0x0003
// SPI 0x55AA 0x0004
// I2C 0x55AA 0x0005
// OTP 0x55AA 0x0006
// Wait 0x55AA 0x0007
// Wait 0x55AA 0x0008
// SARAM 0x55AA 0x000A <-- "Boot to SARAM"
// Flash 0x55AA 0x000B
// Wait 0x55AA Other
//
// Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger
// according to the Boot Mode Table above. Build/Load project,
// Reset the device, and Run example
//
// $End_Boot_Table
//
// DESCRIPTION:
//
// This example modifies the MEP control registers to show edge
// displacement due to the HRPWM control extension of the respective
// EPwm module
// All EPwm1A,2A,3A,4A channels (GPIO0, GPIO2, GPIO4, GPIO6) will have
// fine edge movement due to HRPWM logic
//
// 1. PWM Freq = SYSCLK/(period=10),
// ePWM1A toggle low/high with MEP control on rising edge
// PWM Freq = SYSCLK/(period=10),
// ePWM1B toggle low/high with NO HRPWM control
//
// 2. PWM Freq = SYSCLK/(period=20),
// ePWM2A toggle low/high with MEP control on rising edge
// PWM Freq = SYSCLK/(period=20),
// ePWM2B toggle low/high with NO HRPWM control
//
// 3. PWM Freq = SYSCLK/(period=10),
// ePWM3A toggle as high/low with MEP control on falling edge
// PWM Freq = SYSCLK/(period=10),
// ePWM3B toggle low/high with NO HRPWM control
//
// 4. PWM Freq = SYSCLK/(period=20),
// ePWM4A toggle as high/low with MEP control on falling edge
// PWM Freq = SYSCLK/(period=20),
// ePWM4B toggle low/high with NO HRPWM control
//
//
//###########################################################################
// $TI Release: F2802x Support Library v3.03.00.00 $
// $Release Date: Tue May 26 17:09:17 IST 2020 $
// $Copyright:
// Copyright (C) 2009-2020 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#include "F2802x_Device.h" // f2802x Headerfile
#include "common/include/f2802x_examples.h" // f2802x Examples Headerfile
#include "f2802x_epwm_defines.h" // useful defines for initialization
//
// Function prototypes
//
void HRPWM1_Config(Uint16);
//%%void HRPWM2_Config(Uint16);
//%%void HRPWM3_Config(Uint16);
//%%void HRPWM4_Config(Uint16);
//ADC
__interrupt void adc_isr(void);
void Adc_Config(void);
//
// Globals
//
uint16_t LoopCount;
uint16_t ConversionCount;
uint16_t Voltage1[10];
uint16_t Voltage2[10];
//
// Globals
//
uint16_t i,j,DutyFine,n,update;
uint32_t temp;
//
// Main
//
void main(void)
{
//
// WARNING: Always ensure you call memcpy before running any functions from
// RAM InitSysCtrl includes a call to a RAM based function and without a
// call to memcpy first, the processor will go "into the weeds"
//
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the f2802x_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the f2802x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
//InitGpio(); // Skipped for this example
//
// For this case, just init GPIO for EPwm1-EPwm4
//
//
// For this case just init GPIO pins for EPwm1, EPwm2, EPwm3, EPwm4
// These functions are in the f2802x_EPwm.c file
//
InitEPwm1Gpio();
//%% InitEPwm2Gpio();
//%%InitEPwm3Gpio();
//%%InitEPwm4Gpio();
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the f2802x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in f2802x_DefaultIsr.c.
// This function is found in f2802x_PieVect.c.
//
InitPieVectTable();
//
// Step 4. Initialize all the Device Peripherals:
// Not required for this example
//
//
// For this example, only initialize the EPwm
// Step 5. User specific code, enable interrupts:
//
update =1;
DutyFine =0;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
//
// WARNING: Always ensure you call memcpy before running any functions from
// RAM InitSysCtrl includes a call to a RAM based function and without a
// call to memcpy first, the processor will go "into the weeds"
//
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the f2802x_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the f2802x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
//InitGpio(); // Skipped for this example
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the f2802x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in f2802x_DefaultIsr.c.
// This function is found in f2802x_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// Step 4. Initialize all the Device Peripherals
//
InitAdc(); // For this example, init the ADC
AdcOffsetSelfCal();
//
// Step 5. User specific code, enable interrupts:
// Enable ADCINT1 in PIE
//
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
IER |= M_INT1; // Enable CPU Interrupt 1
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
LoopCount = 0;
ConversionCount = 0;
//
// Configure ADC
// Note: Channel ADCINA4 will be double sampled to workaround the ADC 1st
// sample issue for rev0 silicon errata
//
EALLOW;
//
// ADCINT1 trips after AdcResults latch
//
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1;
AdcRegs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
//
// setup EOC2 to trigger ADCINT1 to fire
//
AdcRegs.INTSEL1N2.bit.INT1SEL = 2;
//
// set SOC0 channel select to ADCINA1
//
AdcRegs.ADCSOC0CTL.bit.CHSEL = 1;
//
// set SOC1 channel select to ADCINA1
//
AdcRegs.ADCSOC1CTL.bit.CHSEL = 1;
//
// set SOC1 channel select to ADCINA0
//
AdcRegs.ADCSOC2CTL.bit.CHSEL = 0;
//
// set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts first
// then SOC1
//
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5;
//
// set SOC1 start trigger on EPWM1A, due to round-robin SOC0 converts first
// then SOC1
//
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5;
//
// set SOC2 start trigger on EPWM1A, due to round-robin SOC0 converts first
// then SOC1, then SOC2
//
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 5;
//
// set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
//
AdcRegs.ADCSOC0CTL.bit.ACQPS = 6;
//
// set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
//
AdcRegs.ADCSOC1CTL.bit.ACQPS = 6;
//
// set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
//
AdcRegs.ADCSOC2CTL.bit.ACQPS = 6;
EDIS;
//
// Assumes ePWM2 clock is already enabled in InitSysCtrl();
//
EPwm2Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
//
// Select SOC from from CPMA on upcount
//
EPwm2Regs.ETSEL.bit.SOCASEL = 4;
EPwm2Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm2Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm2Regs.TBPRD = 0xFFFF; // Set period for ePWM1
EPwm2Regs.TBCTL.bit.CTRMODE = 0; // count up and start
//
// Wait for ADC interrupt
//
for(;;)
{
LoopCount++;
}
}
//
// adc_isr -
//
__interrupt void
adc_isr(void)
{
//
// discard ADCRESULT0 as part of the workaround to the 1st sample errata
// for rev0
//
Voltage1[ConversionCount] = AdcResult.ADCRESULT1;
Voltage2[ConversionCount] = AdcResult.ADCRESULT2;
//
// If 20 conversions have been logged, start over
//
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else
{
ConversionCount++;
}
//
// Clear ADCINT1 flag reinitialize for next SOC
//
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
//
// Acknowledge interrupt to PIE
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
return;
if(Voltage1[ConversionCount]>=3000)
{ HRPWM1_Config(4);
}
else
{HRPWM1_Config(10);
}
//
// Some useful Period vs Frequency values
// SYSCLKOUT = 60 MHz
//
// Period Frequency
// 1000 60 kHz
// 800 75 kHz
// 600 100 kHz
// 500 120 kHz
// 250 240 kHz
// 200 300 kHz
// 100 600 kHz
// 50 1.2 Mhz
// 25 2.4 Mhz
// 20 3.0 Mhz
// 12 5.0 MHz
// 10 6.0 MHz
// 9 6.7 MHz
// 8 7.5 MHz
// 7 8.6 MHz
// 6 10.0 MHz
// 5 12.0 MHz
//
// ePWM and HRPWM register initialization
//
// ePWM1 target, Period = 4
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
while (update ==1)
{
for(DutyFine =1; DutyFine <256 ;DutyFine ++)
{
//
// Example, write to the HRPWM extension of CMPA
//
//
// Left shift by 8 to write into MSB bits
//
EPwm1Regs.CMPA.half.CMPAHR = DutyFine << 8;
//
// Left shift by 8 to write into MSB bits
for (i=0;i<10000;i++)
{
//
// Dummy delay between MEP changes
//
}
}
}
}
//
// HRPWM1_Config -
//
void
HRPWM1_Config(Uint16 period)
{
//
// ePWM1 register configuration with HRPWM
// ePWM1A toggle low/high with MEP control on Rising edge
//
EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE; // set Immediate load
EPwm1Regs.TBPRD = period-1; // PWM frequency = 1 / period
EPwm1Regs.CMPA.half.CMPA = period / 2; // set duty 50% initially
EPwm1Regs.CMPA.half.CMPAHR = (1 << 8); // initialize HRPWM extension
EPwm1Regs.CMPB = period / 2; // set duty 50% initially
EPwm1Regs.TBPHS.all = 0;
EPwm1Regs.TBCTR = 0;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // EPwm1 is the Master
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR; // PWM toggle low/high
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;
EPwm1Regs.AQCTLB.bit.ZRO = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;
EALLOW;
EPwm1Regs.HRCNFG.all = 0x0;
EPwm1Regs.HRCNFG.bit.EDGMODE = HR_REP; // MEP control on Rising edge
EPwm1Regs.HRCNFG.bit.CTLMODE = HR_CMP;
EPwm1Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO;
EDIS;
}
//
// End of File
//