This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Hi Team,
My customer used F280049 CLA software resolver library Resolver_Lib_CLA_Float.lib, and reported an "#17003-D Warning", while removed the Resolver_Lib_CLA_Float.lib file, this warning removed; also has enlarger the size of CLA_scratchpad_SIZE and not removed the file, the warning still existed;
Description Resource Path Location Type
<a href="processors.wiki.ti.com/.../17003"> relocation to symbol "CLAscratch_end" overflowed; the 5-bit relocated address 0xf6 is too large to encode in the 16-bit unsigned field (type = 'R_ABS16_OC' (107), file = "../12_CLA/lib/Resolver_Lib_CLA_float.lib<Resolver_CLA_Source.obj>", offset = 0x00000326, section = "Cla1Prog") SD100_7300 C/C++ Problem
could you kindly give comments on how to remove the warning? Expect for your reply, thanks.
Best Regards
Benjamin
Benjamin,
What does the user's linker command file look like for the CLA sections? I would double check that they are using valid memory for the CLA as a first step.
Regards
Lori
Hi lori,
Attached is the CMD file, could you kindly double check it? Expect for your reply, thanks.
// Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x0000F3, length = 0x00030D RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ /* BANK 0 */ FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */ FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x00F80 /* on-chip Flash */ CSM_RSVD : origin = 0x08FF82, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ CSM_PWL_P0 : origin = 0x08FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ /* BANK 1 */ FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0 /* on-chip Flash */ FPUTABLES : origin = 0x3F9200, length = 0x001800 /* FPU Tables in Boot ROM */ // IQTABLES : origin = 0x3F0800, length = 0x000F00 /* IQ Math Tables in Boot ROM */ // IQTABLES2 : origin = 0x3F1700, length = 0x000100 /* IQ Math Tables in Boot ROM */ // IQTABLES3 : origin = 0x3F1800, length = 0x000100 /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FEB22, length = 0x000B13 /* Boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMLS6 : origin = 0x00B000, length = 0x000800 RAMLS7 : origin = 0x00B800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x002000 RAMGS1 : origin = 0x00E000, length = 0x002000 RAMGS2 : origin = 0x010000, length = 0x002000 RAMGS3 : origin = 0x012000, length = 0x001FF8 // RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 // CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */ // CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */ } SECTIONS { .cinit : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .text : >>FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC4 | FLASH_BANK0_SEC5 | FLASH_BANK0_SEC6 | FLASH_BANK0_SEC7 | FLASH_BANK0_SEC8 | FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10 | FLASH_BANK0_SEC11 | FLASH_BANK0_SEC12 , PAGE = 0, ALIGN(4) codestart : > BEGIN PAGE = 0, ALIGN(4) .stack : > RAMM1 PAGE = 1 .switch : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) #if defined(__TI_EABI__) .init_array : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .bss : > RAMLS5, PAGE = 1 .bss:output : > RAMLS5, PAGE = 1 .bss:cio : > RAMLS5, PAGE = 1 .data : > RAMLS6, PAGE = 1 .sysmem : > RAMLS6, PAGE = 1 .const : >> FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15, PAGE = 0, ALIGN(4) #else .pinit : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .ebss : >>RAMLS5 | RAMLS6 | RAMLS7 | RAMGS0 , PAGE = 1 .esysmem : > RAMLS6, PAGE = 1 .cio : > RAMLS5, PAGE = 1 .econst : >>FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15, PAGE = 0, ALIGN(4) #endif ramgs0 : > RAMGS0, PAGE = 1 ramgs1 : > RAMGS1, PAGE = 1 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ csmpasswds : > CSM_PWL_P0, PAGE = 0 csm_rsvd : > CSM_RSVD, PAGE = 0 /* Allocate IQ math areas: */ // IQmath : > FLASH_BANK0_SEC13, PAGE = 0 /* Math Code */ // IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate IQ math areas: */ IQmath : > FLASH_BANK1_SEC2, PAGE = 0, ALIGN(8) /* Math Code */ IQmathTables : > FLASH_BANK1_SEC3, PAGE = 0, ALIGN(8) /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD debug_buffer : > RAMGS3, PAGE = 1 vectors : > VECTORS, PAGE = 0, TYPE = DSECT #if defined(__TI_EABI__) /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK1_SEC0, RUN = RAMLS0, LOAD_START(Cla1ProgLoadStart), RUN_START(Cla1ProgRunStart), LOAD_SIZE(Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #else /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK1_SEC0, RUN = RAMLS0, LOAD_START(_Cla1ProgLoadStart), RUN_START(_Cla1ProgRunStart), LOAD_SIZE(_Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #endif Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 #if defined(__TI_EABI__) .TI.ramfunc : LOAD = FLASH_BANK0_SEC0, RUN = RAMLS4 LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0, ALIGN(4) #else .TI.ramfunc : LOAD = FLASH_BANK0_SEC0, RUN = RAMLS4 LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #endif .scratchpad : >> RAMGS1 | RAMGS2 | RAMGS3 , PAGE = 1 // .scratchpad : > RAMGS1, PAGE = 1 .bss_cla : > RAMLS1, PAGE = 1 Cla1DataRam : > RAMLS2, PAGE = 1 cla_shared : > RAMLS1, PAGE = 1 CLAmathTables : > RAMLS1, PAGE = 1 CLA1mathTables : > RAMLS1, PAGE = 1 #if defined(__TI_EABI__) .const_cla : LOAD = FLASH_BANK1_SEC2, RUN = RAMLS3, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #else .const_cla : LOAD = FLASH_BANK1_SEC2, RUN = RAMLS3, RUN_START(_Cla1ConstRunStart), LOAD_START(_Cla1ConstLoadStart), LOAD_SIZE(_Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #endif CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMGS3, PAGE = 1, ALIGN=2 } /* //=========================================================================== // End of file. //=========================================================================== */
Best Regards
Benjamin
Benjamin,
The CLA's .scratchpad is allocated to GSx memory which is not accessible by the CLA. Refer to the memory map in the device data sheet.
Regards
Lori
Hi Lori,
I have the same customer with Benjamin, I told customer what you advised, and customer revised cmd twice as attach files, but the problem still unsolved.
Could you please double check it?
Thank you so much!
CLA_SCRATCHPAD_SIZE = 0x200; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x0000F3, length = 0x00030D RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ /* BANK 0 */ FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */ FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x00F80 /* on-chip Flash */ CSM_RSVD : origin = 0x08FF82, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ CSM_PWL_P0 : origin = 0x08FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ /* BANK 1 */ FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x004000 /* on-chip Flash */ FLASH_BANK1_SEC1 : origin = 0x094000, length = 0x004000 /* on-chip Flash */ FLASH_BANK1_SEC2 : origin = 0x098000, length = 0x004000 /* on-chip Flash */ FLASH_BANK1_SEC3 : origin = 0x09C000, length = 0x002000 /* on-chip Flash */ FLASH_BANK1_SEC4 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC5 : origin = 0x09F000, length = 0x000FF0 /* on-chip Flash */ FPUTABLES : origin = 0x3F9200, length = 0x001800 /* FPU Tables in Boot ROM */ // IQTABLES : origin = 0x3F0800, length = 0x000F00 /* IQ Math Tables in Boot ROM */ // IQTABLES2 : origin = 0x3F1700, length = 0x000100 /* IQ Math Tables in Boot ROM */ // IQTABLES3 : origin = 0x3F1800, length = 0x000100 /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FEB22, length = 0x000B13 /* Boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMLS6 : origin = 0x00B000, length = 0x000800 RAMLS7 : origin = 0x00B800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x002000 RAMGS1 : origin = 0x00E000, length = 0x002000 RAMGS2 : origin = 0x010000, length = 0x002000 RAMGS3 : origin = 0x012000, length = 0x001FF8 // RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } SECTIONS { .cinit : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .text : >>FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC4 | FLASH_BANK0_SEC5 | FLASH_BANK0_SEC6 | FLASH_BANK0_SEC7 | FLASH_BANK0_SEC8 | FLASH_BANK0_SEC9 | FLASH_BANK0_SEC10 | FLASH_BANK0_SEC11 | FLASH_BANK0_SEC12 , PAGE = 0, ALIGN(4) codestart : > BEGIN PAGE = 0, ALIGN(4) .stack : > RAMM1 PAGE = 1 .switch : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) #if defined(__TI_EABI__) .init_array : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .bss : > RAMLS5, PAGE = 1 .bss:output : > RAMLS5, PAGE = 1 .bss:cio : > RAMLS5, PAGE = 1 .data : > RAMLS6, PAGE = 1 .sysmem : > RAMLS6, PAGE = 1 .const : >> FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15, PAGE = 0, ALIGN(4) #else .pinit : > FLASH_BANK0_SEC0, PAGE = 0, ALIGN(4) .ebss : >>RAMLS5 | RAMLS6 | RAMLS7 | RAMGS0 , PAGE = 1 .esysmem : > RAMLS6, PAGE = 1 .cio : > RAMLS5, PAGE = 1 .econst : >>FLASH_BANK0_SEC14 | FLASH_BANK0_SEC15, PAGE = 0, ALIGN(4) #endif ramgs0 : > RAMGS0, PAGE = 1 ramgs1 : > RAMGS1, PAGE = 1 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ csmpasswds : > CSM_PWL_P0, PAGE = 0 csm_rsvd : > CSM_RSVD, PAGE = 0 /* Allocate IQ math areas: */ // IQmath : > FLASH_BANK0_SEC13, PAGE = 0 /* Math Code */ // IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate IQ math areas: */ IQmath : > FLASH_BANK1_SEC2, PAGE = 0, ALIGN(8) /* Math Code */ IQmathTables : > FLASH_BANK1_SEC3, PAGE = 0, ALIGN(8) /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD debug_buffer : > RAMGS3, PAGE = 1 vectors : > VECTORS, PAGE = 0, TYPE = DSECT #if defined(__TI_EABI__) /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK1_SEC0, RUN = RAMLS0, LOAD_START(Cla1ProgLoadStart), RUN_START(Cla1ProgRunStart), LOAD_SIZE(Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #else /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK1_SEC0, RUN = RAMLS0, LOAD_START(_Cla1ProgLoadStart), RUN_START(_Cla1ProgRunStart), LOAD_SIZE(_Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #endif Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 #if defined(__TI_EABI__) .TI.ramfunc : LOAD = FLASH_BANK0_SEC0, RUN = RAMLS4 LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0, ALIGN(4) #else .TI.ramfunc : LOAD = FLASH_BANK0_SEC0, RUN = RAMLS4 LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #endif .scratchpad : > RAMLS0, PAGE = 0 .bss_cla : > RAMLS1, PAGE = 1 Cla1DataRam : > RAMLS2, PAGE = 1 cla_shared : > RAMLS1, PAGE = 1 CLAmathTables : > RAMLS1, PAGE = 1 CLA1mathTables : > RAMLS1, PAGE = 1 #if defined(__TI_EABI__) .const_cla : LOAD = FLASH_BANK1_SEC1, RUN = RAMLS3, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #else .const_cla : LOAD = FLASH_BANK1_SEC1, RUN = RAMLS3, RUN_START(_Cla1ConstRunStart), LOAD_START(_Cla1ConstLoadStart), LOAD_SIZE(_Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #endif CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMGS1, PAGE = 1, ALIGN=2 } /* //=========================================================================== // End of file. //=========================================================================== */
CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x0000F3, length = 0x00030D RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ /* BANK 0 */ FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */ FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x004000 /* on-chip Flash */ FLASH_BANK0_SEC3 : origin = 0x086000, length = 0x004000 /* on-chip Flash */ FLASH_BANK0_SEC4 : origin = 0x08A000, length = 0x004000 /* on-chip Flash */ FLASH_BANK0_SEC5 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC6 : origin = 0x08F000, length = 0x00F80 /* on-chip Flash */ CSM_RSVD : origin = 0x08FF82, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ CSM_PWL_P0 : origin = 0x08FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ /* BANK 1 */ FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x000FF0 /* on-chip Flash */ FPUTABLES : origin = 0x3F9200, length = 0x001800 /* FPU Tables in Boot ROM */ // FLASH_BANK1_SEC15_RSVD : origin = 0x09FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMLS6 : origin = 0x00B000, length = 0x000800 RAMLS7 : origin = 0x00B800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x002000 RAMGS1 : origin = 0x00E000, length = 0x002000 RAMGS2 : origin = 0x010000, length = 0x002000 RAMGS3 : origin = 0x012000, length = 0x001FF8 // RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } SECTIONS { .cinit : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4) .text : >>FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC4 , PAGE = 0, ALIGN(4) codestart : > BEGIN PAGE = 0, ALIGN(4) .stack : > RAMM1 PAGE = 1 .switch : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4) #if defined(__TI_EABI__) .init_array : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4) .bss : > RAMLS5, PAGE = 1 .bss:output : > RAMLS5, PAGE = 1 .bss:cio : > RAMLS5, PAGE = 1 .data : > RAMLS6, PAGE = 1 .sysmem : > RAMLS6, PAGE = 1 .const : > FLASH_BANK0_SEC4, PAGE = 0, ALIGN(4) #else .pinit : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4) .ebss : >>RAMLS5 | RAMLS6 | RAMLS7 | RAMGS0 , PAGE = 1 .esysmem : > RAMLS6, PAGE = 1 .cio : > RAMLS5, PAGE = 1 .econst : > FLASH_BANK0_SEC4, PAGE = 0, ALIGN(4) #endif ramgs0 : > RAMGS0, PAGE = 1 ramgs1 : > RAMGS1, PAGE = 1 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ csmpasswds : > CSM_PWL_P0, PAGE = 0 csm_rsvd : > CSM_RSVD, PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASH_BANK0_SEC6, PAGE = 0, ALIGN(8) /* Math Code */ IQmathTables : > FLASH_BANK0_SEC6, PAGE = 0, ALIGN(8) /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD #if defined(__TI_EABI__) /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK0_SEC4, RUN = RAMLS0, LOAD_START(Cla1ProgLoadStart), RUN_START(Cla1ProgRunStart), LOAD_SIZE(Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #else /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK0_SEC4, RUN = RAMLS0, LOAD_START(_Cla1ProgLoadStart), RUN_START(_Cla1ProgRunStart), LOAD_SIZE(_Cla1ProgLoadSize), PAGE = 0, ALIGN(4) #endif Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 #if defined(__TI_EABI__) .TI.ramfunc : LOAD = FLASH_BANK0_SEC1, RUN = RAMLS4 LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0, ALIGN(4) #else .TI.ramfunc : LOAD = FLASH_BANK0_SEC1, RUN = RAMLS4 LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #endif .scratchpad : > RAMLS1, PAGE = 1 .bss_cla : > RAMLS1, PAGE = 1 Cla1DataRam : > RAMLS2, PAGE = 1 cla_shared : > RAMLS1, PAGE = 1 #if defined(__TI_EABI__) .const_cla : LOAD = FLASH_BANK0_SEC2, RUN = RAMLS3, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #else .const_cla : LOAD = FLASH_BANK0_SEC2, RUN = RAMLS3, RUN_START(_Cla1ConstRunStart), LOAD_START(_Cla1ConstLoadStart), LOAD_SIZE(_Cla1ConstLoadSize), PAGE = 0, ALIGN(4) #endif CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMLS1, PAGE = 1, ALIGN=2 } /* //=========================================================================== // End of file. //=========================================================================== */
Chen,
Did the error message change at all? Please provide the whole error or a screenshot of the error. Which compiler version are they using and are they compiling for EABI?
Regards
Lori
Lori,
Thanks so much for your help.
The files as your advices are attached.
Looking forward for your reply.
Chen
Thank you Chen. I am consulting with members of the compiler team and will get back to you.
Chen,
I cannot reproduce their issue. I see their map file includes __cla_scratchpad_end/start. Do you know what they are using those symbols for in their application?
For CLA type 2, the only linker cmd file entry needed for CLA scratch should be below:
.scratchpad : > RAMLS1, PAGE = 1
So if they are not actually using __cla_scratchpad_end/start, then have them remove below entries from their linker cmd file:
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > RAMLS1, PAGE = 1, ALIGN=2
Thanks,
Greg
Hi GregM,
Thanks for your kindly help.
i met the same problems with customer with the same work, porting TMDSRSLVR_v1.0/F28035_CLA to F280049_CLA, including Resolver_CLA_float.lib and Reslover_CLA.h.
customers remove the parts:
CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMLS1, PAGE = 1, ALIGN=2
But the warnings still exist.
I attach my project files for clear understanding of this issue.
Thank you so mcuh!
Hi Lori & Greg,
I have no error before on ccs and f280049, and I finished porting TMDSRSLVR_resolver project f28035 to f280049 based on C28, and it works.
But, when I try to porting f28035_CLA project to f280049, the issue occurred. And next is my steps.
First, I just init the modules like ADC, epwm, DAC(instead of epwm to generate EXC sin signal, I use DAC to output sin signal) and init_CLA as the attach file shows;
Second, configure epwm_CMPA_Int & ISR(postprocess_ISR) and ADC_INT & ISR(resolver_algo_CLA defined in Resolver_Lib_CLA_float.lib) in CLA task2, CLA task1 used to call function init_resolver_CLA (defined in Resolver_Lib_CLA_float.lib).
Finally, the warning occurred after build, with no error just a series of #17003-D warings as same as customer.
And, could you please take a webex meeting with Benjamin and me? we have to solve this urgent problem!
Thank you so much.
Hi Greg,
Thanks so much for your time and patient help.
it a __cla_scratchpad_end/start problem, as your advice i revised below codes to cmd, and the #17003-D warnings are removed.
// GREG: added below from F28035_FLASH_Resolver.CMD CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start // GREG: added below also from F28035_FLASH_Resolver.CMD // and changed from >RAML2 to >RAMLS1 CLAscratch : { *.lib(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.lib(CLAscratch_end) } > RAMLS1, /* RAML2,*/ PAGE = 1
thank you so much again.